ExportWeldBuilderOutputType Enumeration

NXOpen.Weld.ExportWeldBuilder.OutputType is an alias for NXOpen.Weld.ExportWeldBuilderOutputType

class NXOpen.Weld.ExportWeldBuilderOutputType

Bases: object

the Output Type enum

Enum Members

Enum Member Enum Member Description
IntermediateFile
InformationWindow
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.