EdgePrepValuesBuilderOption Enumeration¶
NXOpen.Weld.EdgePrepValuesBuilder.Option is an alias for NXOpen.Weld.EdgePrepValuesBuilderOption
-
class
NXOpen.Weld.
EdgePrepValuesBuilderOption
¶ Bases:
object
Option to indicate how the values are to be used.
Enum Members
Enum Member Enum Member Description Entered Use the values entered as edge prep values. Computed Use the computed values as edge prep values. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-