EasyPatternBuilderPlaneMethodTypes Enumeration¶
NXOpen.Weld.EasyPatternBuilder.PlaneMethodTypes is an alias for NXOpen.Weld.EasyPatternBuilderPlaneMethodTypes
-
class
NXOpen.Weld.
EasyPatternBuilderPlaneMethodTypes
¶ Bases:
object
The plane to cut sections in to determine placement measurement patterns.
Enum Members
Enum Member Enum Member Description InferPlanes Determine the best XC,YC, or ZC plane. ParallelXCPlanes Patterns are on the XC plane. ParallelYCPlanes Patterns are on the YC plane. ParallelZCPlanes Patterns are on the ZC plane. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-