EasyPatternBuilderHemMethodTypes Enumeration¶
NXOpen.Weld.EasyPatternBuilder.HemMethodTypes is an alias for NXOpen.Weld.EasyPatternBuilderHemMethodTypes
-
class
NXOpen.Weld.
EasyPatternBuilderHemMethodTypes
¶ Bases:
object
Indicates the method to use to compute the hem vector location.
Enum Members
Enum Member Enum Member Description MidPoint Use the mid point of a section cut. NormalToBody Use Normal to Body Method. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-