DatumCommonBuilderSolidTypes Enumeration¶
NXOpen.Weld.DatumCommonBuilder.SolidTypes is an alias for NXOpen.Weld.DatumCommonBuilderSolidTypes
-
class
NXOpen.Weld.
DatumCommonBuilderSolidTypes
¶ Bases:
object
Settings for defining the solid type to create for the datum object.
Enum Members
Enum Member Enum Member Description Sphere Datum solid will be a sphere Cylinder Datum solid will be a cylinder Cone Datum solid will be a cone -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-