DatumCommonBuilderCustomTypes Enumeration¶
NXOpen.Weld.DatumCommonBuilder.CustomTypes is an alias for NXOpen.Weld.DatumCommonBuilderCustomTypes
-
class
NXOpen.Weld.
DatumCommonBuilderCustomTypes
¶ Bases:
object
The custom type of the datum specified for creation.
Enum Members
Enum Member Enum Member Description Default A datum surface or pin specified in the customer defaults by the Default type. Custom1 A datum surface or pin specified in the customer defaults by the Custom1 type. Custom2 A datum surface or pin specified in the customer defaults by the Custom2 type. Custom3 A datum surface or pin specified in the customer defaults by the Custom3 type. Custom4 A datum surface or pin specified in the customer defaults by the Custom4 type. Custom5 A datum surface or pin specified in the customer defaults by the Custom5 type. Custom6 A datum surface or pin specified in the customer defaults by the Custom6 type. Custom7 A datum surface or pin specified in the customer defaults by the Custom7 type. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-