VisualReportReportingObjectTypeOption Enumeration¶
NXOpen.VisualReporting.VisualReport.ReportingObjectTypeOption is an alias for NXOpen.VisualReporting.VisualReportReportingObjectTypeOption
-
class
NXOpen.VisualReporting.
VisualReportReportingObjectTypeOption
¶ Bases:
object
Represents the possible
NXOpen.VisualReporting.VisualReport.ReportingObjectType()
for aNXOpen.VisualReporting.VisualReport
. Only valid if theNXOpen.VisualReporting.VisualReport.ScopeType()
of theNXOpen.VisualReporting.VisualReport
isNXOpen.VisualReporting.VisualReportScopeTypeOption.Component
type.Enum Members
Enum Member Enum Member Description Part The reporting objects are parts. Component The reporting objects are components. Inferred The reporting objects are inferred from the properties used in the report. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-