VisualReportObjectTypeOption Enumeration¶
NXOpen.VisualReporting.VisualReport.ObjectTypeOption is an alias for NXOpen.VisualReporting.VisualReportObjectTypeOption
-
class
NXOpen.VisualReporting.
VisualReportObjectTypeOption
¶ Bases:
object
Represents the possible report object type options for a
NXOpen.VisualReporting.VisualReport
. Only valid if theNXOpen.VisualReporting.VisualReport.ScopeType()
of theNXOpen.VisualReporting.VisualReport
isNXOpen.VisualReporting.VisualReportScopeTypeOption.SubPart
type.Enum Members
Enum Member Enum Member Description Body The report objects are bodies Face The report objects are faces -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-