VisualReportExplorerReportOnObjectsOption Enumeration¶
NXOpen.VisualReporting.VisualReportExplorer.ReportOnObjectsOption is an alias for NXOpen.VisualReporting.VisualReportExplorerReportOnObjectsOption
-
class
NXOpen.VisualReporting.
VisualReportExplorerReportOnObjectsOption
¶ Bases:
object
When the set of objects to report upon is changed, should the contents of the set be replaced or extended.
Enum Members
Enum Member Enum Member Description Replace Replace the existing set of objects Add Add to the existing set of objects -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-