VisualReportBuilderPropertyUsageOption Enumeration¶
NXOpen.VisualReporting.VisualReportBuilder.PropertyUsageOption is an alias for NXOpen.VisualReporting.VisualReportBuilderPropertyUsageOption
-
class
NXOpen.VisualReporting.
VisualReportBuilderPropertyUsageOption
¶ Bases:
object
Represents the usage option of reference
NXOpen.VisualReporting.Property
Enum Members
Enum Member Enum Member Description Tooltip The property is used in tooltip only InfoView The property is used in info view only TooltipAndInfoView -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-