PropertyTypeOption Enumeration¶
NXOpen.VisualReporting.Property.TypeOption is an alias for NXOpen.VisualReporting.PropertyTypeOption
-
class
NXOpen.VisualReporting.
PropertyTypeOption
¶ Bases:
object
Represents the possible
NXOpen.VisualReporting.Property.PropertyType()
options for a propertyEnum Members
Enum Member Enum Member Description ArrangementSpecificPositionProperty Arrangement specific positioning AttributeProperty Part attribute property ComponentGroupProperty Component group name ComponentNameProperty Component name DescriptivePartNameProperty Descriptive part name LoadStateProperty The load state of the component MassKgProperty The mass of the component in pounds MassLbProperty The mass of the component in kilograms ModifiedProperty Whether the component is modified MultiCadProperty Parts mastered in a CAD system other than NX PartNameProperty Part name PartUnitsProperty Part units PiecePartProperty Piece part PositionProperty The position of the component PositionControlProperty The position control of the component ReadOnlyProperty Whether the component is read-only ReferenceSetProperty The reference set used by the component RootPartProperty Root part occurrence SuppressionControlProperty The suppression control of the component WeightStatusProperty The weight status of the component TeamcenterProperty Teamcenter property ServerProperty Server Property defined in server side report DegreesOfFreedomProperty The freedom degree of the component RuleEvaluationResultProperty Rule Evaluation for results in part CheckMateResultProperty Check-Mate result LastModifiedDateProperty last modify date property RequirementsValidationStatusProperty Requirement validate result RepresentationProperty Representation Status LastModifiedUserProperty last modify user property ComponentProperty Assembly Navigator column property MassGmProperty The mass of the component in grams PartFamilyMemberProperty Part family member LinkedPartProperty Linked part ProductTemplateProperty Product Template BodyDensityProperty Body density property BodyMassProperty Body mass property BodyRadiusGyrationProperty Body radius gyration property BodySurfaceAreaProperty Body surface area property BodyTypeProperty Body type property BodyVolumeProperty Body volume property BodyWeightProperty Body weight property FaceAreaProperty Face area property FaceTypeProperty Face type property FaceMinRadiusProperty Face minimum radius property FacePerimeterProperty Face perimeter property FacePMIFCFProperty Face PMI FCF property FacePMIFCFCharacteristicsProperty Face PMI FCF characteristics property FacePMIFCFCharFormTolProperty Face PMI FCF form characteristics property FacePMIFCFCharLocationTolProperty Face PMI FCF location characteristics property FacePMIFCFCharOrientationTolProperty Face PMI FCF orientation characteristics property FacePMIFCFCharProfileTolProperty Face PMI FCF profile characteristics property FacePMIFCFCharRunoutTolProperty Face PMI FCF run out characteristics property FacePMIDatumFeatureProperty Face PMI datum feature property FacePMIDatumTargetProperty Face PMI datum target property ObjectAttributeProperty Subpart object attribute property ObjectCreatedByUserProperty Subpart object created by user property ObjectCreatedDateProperty Subpart object created date property ObjectCreatedVersionProperty Subpart object created version property ObjectRefByWaveLinkProperty Subpart object referenced by Wave link property ObjectWaveLinkedProperty Subpart object Wave linked property ObjectModifiedByUserProperty Subpart object modified by user property ObjectModifiedDateProperty Subpart object modified date property ObjectModifiedVersionProperty Subpart object modified version property PartitionMembershipProperty Partition Membership property ComponentAddedDateProperty Component Added Date TeamcenterObjectProperty Teamcenter Object property ComponentPatternTypeProperty Component Pattern Type property ObjectNameProperty Subpart object name property NXOpenProperty NX Open property SheetMetalBendAngleProperty Sheet Metal Bend Angle Property SheetMetalBendRadiusProperty Sheet Metal Bend Radius Property SheetMetalFaceTypeAllProperty Sheet Metal All Face Type Property SheetMetalFaceTypeBendProperty Sheet Metal Bend Face Type Property SheetMetalFaceTypeDeformProperty Sheet Metal Deform Face Type Property SheetMetalFaceTypeWebProperty Sheet Metal Web Face Type Property SheetMetalNeutralFactorProperty Sheet Metal Neutral Factor Property SheetMetalBodyTypeProperty Sheet Metal Body Type Property FeatureFailureProperty Feature failure component property -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-