PropertyDatatypeOption Enumeration¶
NXOpen.VisualReporting.Property.DatatypeOption is an alias for NXOpen.VisualReporting.PropertyDatatypeOption
-
class
NXOpen.VisualReporting.
PropertyDatatypeOption
¶ Bases:
object
Represents the possible
NXOpen.VisualReporting.Property.SystemDatatype()
options for a property.Enum Members
Enum Member Enum Member Description String String data type Integer Integer data type Real Floating point data type Boolean Boolean data type Unknown The data type is unknown Null Null data type Date Date data type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-