GroupLabelTagPriorityOption Enumeration¶
NXOpen.VisualReporting.GroupLabel.TagPriorityOption is an alias for NXOpen.VisualReporting.GroupLabelTagPriorityOption
-
class
NXOpen.VisualReporting.
GroupLabelTagPriorityOption
¶ Bases:
object
Represents the possible priority options for a
NXOpen.VisualReporting.GroupLabel
.Enum Members
Enum Member Enum Member Description Low Low priority Medium Medium priority High Hign priority -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-