GroupLabelDisplayStyleOption Enumeration¶
NXOpen.VisualReporting.GroupLabel.DisplayStyleOption is an alias for NXOpen.VisualReporting.GroupLabelDisplayStyleOption
-
class
NXOpen.VisualReporting.
GroupLabelDisplayStyleOption
¶ Bases:
object
Represents the possible display style options for a
NXOpen.VisualReporting.GroupLabel
.Enum Members
Enum Member Enum Member Description DeEmphasis Matching objects will be de-emphasized SpecifiedColor Matching objects will be shown using NXOpen.VisualReporting.GroupLabel.Color()
OriginalColor Matching objects will be shown using their original color AutomaticColor Matching objects will be shown using NXOpen.VisualReporting.GroupLabel.Color()
which is system determined-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-