ConditionTypeOption Enumeration¶
NXOpen.VisualReporting.Condition.TypeOption is an alias for NXOpen.VisualReporting.ConditionTypeOption
-
class
NXOpen.VisualReporting.
ConditionTypeOption
¶ Bases:
object
Represents the possible type options for a
NXOpen.VisualReporting.Condition
. If the type is aNXOpen.VisualReporting.ConditionTypeOption.ValueCondition
the type of value can be found fromNXOpen.VisualReporting.Condition.Datatype()
.Enum Members
Enum Member Enum Member Description AndCondition OrCondition NotCondition ValueCondition -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-