ConditionOperatorOption Enumeration¶
NXOpen.VisualReporting.Condition.OperatorOption is an alias for NXOpen.VisualReporting.ConditionOperatorOption
-
class
NXOpen.VisualReporting.
ConditionOperatorOption
¶ Bases:
object
Represents the possible operator type options. for a
NXOpen.VisualReporting.Condition
.Enum Members
Enum Member Enum Member Description EqualOperator LessThanOperator NotLessThanOperator GreaterThanOperator NotGreaterThanOperator NotEqualOperator RegularExpressionOperator ContainsOperator DoesNotContainOperator OnOrBeforeOperator OnOrAfterOperator -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-