ViewCanned Enumeration¶
NXOpen.View.Canned is an alias for NXOpen.ViewCanned
-
class
NXOpen.
ViewCanned
¶ Bases:
object
Describes a simplified indexing scheme for accessing canned views with interfaces that use this enum as a parameter.
Enum Members
Enum Member Enum Member Description Top Front Right Back Bottom Left Isometric Trimetric -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-