ValidationInputType Enumeration¶
NXOpen.Validation.InputType is an alias for NXOpen.ValidationInputType
-
class
NXOpen.
ValidationInputType
¶ Bases:
object
Specifies the input type
Enum Members
Enum Member Enum Member Description KfClass Input rules are in a KF class Spreadsheet Input rules are from a spreadsheet TextFile Input rules are from a text file Xml Input rules are from XML file Tcr Input rules are from TcR Application Input rules are from validation applications Num Last item define the number of the input source, not used as a type. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-