XmlComparatorResult Enumeration¶
NXOpen.Validate.XmlComparator.Result is an alias for NXOpen.Validate.XmlComparatorResult
-
class
NXOpen.Validate.
XmlComparatorResult
¶ Bases:
object
Specifies result of the comparison
Enum Members
Enum Member Enum Member Description Identical Represents two xml files are identical Different Represents two xml files are different -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-