ValidationManager Class¶
-
class
NXOpen.Validate.
ValidationManager
¶ Bases:
object
Represents an object that manages validator and parser associated instance objects.
It handles the creation of new validators and parsers. The ValidationManager also provides
NXOpen.Validate.ValidationManager.FindValidator()
to get validators in current session.To obtain an instance of this class, refer to
NXOpen.Session
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CreateParser | Creates a parser. |
CreateValidator | Creates a validator. |
DeleteParser | Deletes a parser. |
DeleteValidator | Deletes a validator. |
FindParser | Finds parsers in current session. |
FindValidator | Finds validators in current session. |
Method Detail¶
CreateParser¶
-
ValidationManager.
CreateParser
¶ Creates a parser.
Signature
CreateParser(name)
Parameters: name (str) – name of the parser Returns: Return type: NXOpen.Validate.Parser
New in version NX7.5.0.
License requirements: None.
CreateValidator¶
-
ValidationManager.
CreateValidator
¶ Creates a validator.
Signature
CreateValidator(name)
Parameters: name (str) – name of the validator Returns: Return type: NXOpen.Validate.Validator
New in version NX7.5.0.
License requirements: ug_checkmate (“UG Check Mate”)
DeleteParser¶
-
ValidationManager.
DeleteParser
¶ Deletes a parser.
Signature
DeleteParser(parser)
Parameters: parser ( NXOpen.Validate.Parser
) –New in version NX7.5.0.
License requirements: None.
DeleteValidator¶
-
ValidationManager.
DeleteValidator
¶ Deletes a validator.
Signature
DeleteValidator(validator)
Parameters: validator ( NXOpen.Validate.Validator
) –New in version NX7.5.0.
License requirements: ug_checkmate (“UG Check Mate”)
FindParser¶
-
ValidationManager.
FindParser
¶ Finds parsers in current session.
It will return all parsers with the same name.
Signature
FindParser(name)
Parameters: name (str) – Returns: Return type: list of NXOpen.Validate.Parser
New in version NX7.5.0.
License requirements: None.
FindValidator¶
-
ValidationManager.
FindValidator
¶ Finds validators in current session.
It will return all validators with the same name.
Signature
FindValidator(name)
Parameters: name (str) – Returns: Return type: list of NXOpen.Validate.Validator
New in version NX7.5.0.
License requirements: ug_checkmate (“UG Check Mate”)