RequirementBuilderRelationalOperatorOptions Enumeration

NXOpen.Validate.RequirementBuilder.RelationalOperatorOptions is an alias for NXOpen.Validate.RequirementBuilderRelationalOperatorOptions

class NXOpen.Validate.RequirementBuilderRelationalOperatorOptions

Bases: object

This enum represents the relational operator for comparing values

Enum Members

Enum Member Enum Member Description
Equal
NotEqual
LessThan
LessThanOrEqual
GreaterThan
GreaterThanOrEqual
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.