RequirementBuilderDefinitionMethodOptions Enumeration

NXOpen.Validate.RequirementBuilder.DefinitionMethodOptions is an alias for NXOpen.Validate.RequirementBuilderDefinitionMethodOptions

class NXOpen.Validate.RequirementBuilderDefinitionMethodOptions

Bases: object

This enum represents the type of requirement definition method

Enum Members

Enum Member Enum Member Description
SingleSidedComparison
DoubleSidedComparison
SetOfValues
Formula
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.