PartNode Class¶
-
class
NXOpen.Validate.
PartNode
¶ Bases:
NXOpen.TransientObject
Represents a part file that validator will check against.
Part node contains the information of part filename and part object. You can create the part node by inputting part filename, or by inputting part object, or by inputting both. Validator will use the part object in the part node for checking. Only when the part object in the part node is None, then validator will use the part filename for checking.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
FileName | Returns or sets the part file name |
PartObject | Returns or sets the part object |
Property Detail¶
FileName¶
-
PartNode.
FileName
¶ Returns or sets the part file name
-------------------------------------
Getter Method
Signature
FileName
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileName
Parameters: fileName (str) – New in version NX7.5.0.
License requirements: None.
PartObject¶
-
PartNode.
PartObject
¶ Returns or sets the part object
-------------------------------------
Getter Method
Signature
PartObject
Returns: Return type: NXOpen.Part
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartObject
Parameters: partObject ( NXOpen.Part
) –New in version NX7.5.0.
License requirements: None.