OverrideBuilderToStates Enumeration

NXOpen.Validate.OverrideBuilder.ToStates is an alias for NXOpen.Validate.OverrideBuilderToStates

class NXOpen.Validate.OverrideBuilderToStates

Bases: object

Represents the override request to state

Enum Members

Enum Member Enum Member Description
Passed
Failed
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.