OverrideBuilderDecisionActions Enumeration

NXOpen.Validate.OverrideBuilder.DecisionActions is an alias for NXOpen.Validate.OverrideBuilderDecisionActions

class NXOpen.Validate.OverrideBuilderDecisionActions

Bases: object

Represents the override request decision action

Enum Members

Enum Member Enum Member Description
Approved
Rejected
Pending
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.