VRMLImporterFileUnitsType Enumeration¶
NXOpen.VRMLImporter.FileUnitsType is an alias for NXOpen.VRMLImporterFileUnitsType
-
class
NXOpen.
VRMLImporterFileUnitsType
¶ Bases:
object
Specifies the VRML file units.
New in version NX5.0.0.
Enum Members
Enum Member Enum Member Description Meters VRML file is in units of meters. Millimeters VRML file is in units of millimeters. Inches VRML file is in units of inches. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-