NXOpen.UserDefinedObjects Package

Classes

UserDefinedClass Class JA interface for the UserDefinedClass object
UserDefinedClassManager Class JA interface for the UserDefinedClassManager object
UserDefinedDisplayEvent Class Implements the Display Event Object for UDO’s
UserDefinedEvent Class Implements the Event Object for UDO’s
UserDefinedLinkEvent Class Implements the Display Event Object for UDO’s
UserDefinedObject Class JA interface for the UserDefinedObject object
UserDefinedObjectDisplayContext Class This class is used to display User Defined Objects
UserDefinedObjectManager Class This class creates and manages UserDefinedObjects

Enumerations

UserDefinedClassAllowOwnedObjectSelection Enumeration Allow owned object selection on all objects owned by an object of this NXOpen.UserDefinedObjects.UserDefinedClass.
UserDefinedClassAllowQueryClass Enumeration Allow query class from name options for a NXOpen.UserDefinedObjects.UserDefinedObject of this class.
UserDefinedClassSelection Enumeration Allow query class from name options for a NXOpen.UserDefinedObjects.UserDefinedObject.
UserDefinedEventReason Enumeration Available link types for a UserDefinedObject.
UserDefinedObjectLinkStatus Enumeration Status of the object linked to a NXOpen.Features.UserDefinedObjectFeature
UserDefinedObjectLinkType Enumeration Available link types for a NXOpen.Features.UserDefinedObjectFeature.
UserDefinedObjectDisplayContextFacetType Enumeration The enumerated type facet to be displayed
UserDefinedObjectDisplayContextPolyMarker Enumeration This enumerated type specifies the type of marker to be displayed.
UserDefinedObjectDisplayContextStandardTextRef Enumeration This enumerated type specifies the type of reference point used in the text box for standard_text methods.
UserDefinedObjectDisplayContextTextRef Enumeration This enumerated type specifies the type of reference point used in the text box.
UserDefinedObjectDisplayContextTextSize Enumeration Provides a way to specify the size of the desired text, as small, medium or large (normal is a synonym for medium).
UserDefinedObjectDisplayContextViewMode Enumeration The enumerated view mode

Structs

UserDefinedObjectLinkDefinition_Struct Struct Contains the linked object and it’s status along with the type of link.
UserDefinedObjectManagerLinkedUdoDefinition_Struct Struct Used to define a link to a UserDefinedObject