UserDefinedObjectManager Class¶
-
class
NXOpen.UserDefinedObjects.
UserDefinedObjectManager
¶ Bases:
object
This class creates and manages UserDefinedObjects
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateUserDefinedObject | Constructs a new NXOpen.Features.UserDefinedObjectFeature . |
GetLinksToObject | Queries an NX Object to find all UserDefinedObjects.UserDefinedObject ’s that are linked to the given NXObject (note this will not find owning udos) |
GetOwningUserDefinedObject | Queries an NX Object to find the UserDefinedObjects.UserDefinedObject that owns the given NXObject (note this will return null for the owning udo if the object is not owned) |
GetUdosOfClass | Finds all UserDefinedObjects.UserDefinedObject instances that use the given NXOpen.UserDefinedObjects.UserDefinedClass . |
IsObjectLinkable | Queries an NX Object to see if it can be linked to a UserDefinedObjects.UserDefinedObject via the given link type |
IsObjectLinkedToUserDefinedObject | Queries an NX Object to see if it is linked to a UserDefinedObjects.UserDefinedObject (note this will not tell you if the object is owned by a UDO with an owning link) |
IsObjectOwnedByUserDefinedObject | Queries an NX Object to see if it is owned by a UserDefinedObjects.UserDefinedObject |
Structs¶
UserDefinedObjectManagerLinkedUdoDefinition_Struct Struct | Used to define a link to a UserDefinedObject |
Method Detail¶
CreateUserDefinedObject¶
-
UserDefinedObjectManager.
CreateUserDefinedObject
¶ Constructs a new
NXOpen.Features.UserDefinedObjectFeature
.Signature
CreateUserDefinedObject(udoClass)
Parameters: udoClass ( NXOpen.UserDefinedObjects.UserDefinedClass
) – The UserDefinedClass used to define the new UserDefinedObjectReturns: The new UserDefinedObject instance Return type: NXOpen.UserDefinedObjects.UserDefinedObject
New in version NX5.0.0.
License requirements: None.
GetLinksToObject¶
-
UserDefinedObjectManager.
GetLinksToObject
¶ Queries an NX Object to find all
UserDefinedObjects.UserDefinedObject
’s that are linked to the given NXObject (note this will not find owning udos)Signature
GetLinksToObject(linkObject)
Parameters: linkObject ( NXOpen.TaggedObject
) – NXObject to query for linksReturns: The link definitions from UDO’s to the NXObject Return type: list of NXOpen.UserDefinedObjects.UserDefinedObjectManagerLinkedUdoDefinition_Struct
New in version NX5.0.0.
License requirements: None.
GetOwningUserDefinedObject¶
-
UserDefinedObjectManager.
GetOwningUserDefinedObject
¶ Queries an NX Object to find the
UserDefinedObjects.UserDefinedObject
that owns the given NXObject (note this will return null for the owning udo if the object is not owned)Signature
GetOwningUserDefinedObject(linkObject)
Parameters: linkObject ( NXOpen.TaggedObject
) – NXObject to query for an owning UDOReturns: The UDO which owns the NXObject Return type: NXOpen.UserDefinedObjects.UserDefinedObject
New in version NX5.0.0.
License requirements: None.
GetUdosOfClass¶
-
UserDefinedObjectManager.
GetUdosOfClass
¶ Finds all
UserDefinedObjects.UserDefinedObject
instances that use the givenNXOpen.UserDefinedObjects.UserDefinedClass
.Signature
GetUdosOfClass(udoClass)
Parameters: udoClass ( NXOpen.UserDefinedObjects.UserDefinedClass
) – The UserDefinedClass we want to findReturns: User Defined Objects of the given class Return type: list of NXOpen.UserDefinedObjects.UserDefinedObject
New in version NX5.0.0.
License requirements: None.
IsObjectLinkable¶
-
UserDefinedObjectManager.
IsObjectLinkable
¶ Queries an NX Object to see if it can be linked to a
UserDefinedObjects.UserDefinedObject
via the given link typeSignature
IsObjectLinkable(linkObject, linkType)
Parameters: - linkObject (
NXOpen.TaggedObject
) – NXObject to query for linkability - linkType (
NXOpen.UserDefinedObjects.UserDefinedObjectLinkType
) – The link type used to link this object to a UDO
Returns: TRUE - This object can be linked to a UDO with the given link type, FALSE - this object can not be NOT linked to a UDO with the given link type
Return type: bool
New in version NX5.0.0.
License requirements: None.
- linkObject (
IsObjectLinkedToUserDefinedObject¶
-
UserDefinedObjectManager.
IsObjectLinkedToUserDefinedObject
¶ Queries an NX Object to see if it is linked to a
UserDefinedObjects.UserDefinedObject
(note this will not tell you if the object is owned by a UDO with an owning link)Signature
IsObjectLinkedToUserDefinedObject(linkObject)
Parameters: linkObject ( NXOpen.TaggedObject
) – NXObject to query for linksReturns: TRUE - This object is linked to a UDO, FALSE - this object is NOT linked to a UDO Return type: bool New in version NX5.0.0.
License requirements: None.
IsObjectOwnedByUserDefinedObject¶
-
UserDefinedObjectManager.
IsObjectOwnedByUserDefinedObject
¶ Queries an NX Object to see if it is owned by a
UserDefinedObjects.UserDefinedObject
Signature
IsObjectOwnedByUserDefinedObject(linkObject)
Parameters: linkObject ( NXOpen.TaggedObject
) – NXObject to query for an owning UDOReturns: TRUE - This object is owned by a UDO, FALSE - this object is NOT owned by a UDO Return type: bool New in version NX5.0.0.
License requirements: None.