UserDefinedObjectLinkStatus Enumeration¶
NXOpen.UserDefinedObjects.UserDefinedObject.LinkStatus is an alias for NXOpen.UserDefinedObjects.UserDefinedObjectLinkStatus
-
class
NXOpen.UserDefinedObjects.
UserDefinedObjectLinkStatus
¶ Bases:
object
Status of the object linked to a
NXOpen.Features.UserDefinedObjectFeature
Enum Members
Enum Member Enum Member Description UpToDate The associated object is up to date. OutOfDate The associated object is out of date. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-