UserDefinedObjectDisplayContextTextSize Enumeration

NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContext.TextSize is an alias for NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextTextSize

class NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextTextSize

Bases: object

Provides a way to specify the size of the desired text, as small, medium or large (normal is a synonym for medium).

Enum Members

Enum Member Enum Member Description
Small
Normal
Medium
Large
NumSizes
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.