UserDefinedObjectDisplayContextPolyMarker Enumeration¶
NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContext.PolyMarker is an alias for NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextPolyMarker
-
class
NXOpen.UserDefinedObjects.
UserDefinedObjectDisplayContextPolyMarker
¶ Bases:
object
This enumerated type specifies the type of marker to be displayed.
Enum Members
Enum Member Enum Member Description NoMarker Point Dot Asterisk Circle Poundsign X Gridpoint Square TriangleMarker Diamond Centerline ConsFix ConsHorizontal ConsVertical ConsParallel ConsPerpendicular ConsTangent ConsConcentric ConsCoincident ConsCollinear ConsPointOnCurve ConsMidpoint ConsEqualLength ConsEqualRadius ConsConstantLength ConsConstantAngle ConsMirror DimRadius DimDiameter DimParallel DimPerpendicular ConsSlope ConsString ConsUniformScaled ConsNonUniformScaled ConsAssocTrim ConsAssocOffset Disp2tResSpotWeld Disp3tResSpotWeld Disp4tResSpotWeld Disp2tDcSpotWeld Disp3tDcSpotWeld Disp4tDcSpotWeld Disp2tKpcSpotWeld Disp3tKpcSpotWeld Disp4tKpcSpotWeld Disp2tProcSpotWeld Disp3tProcSpotWeld Disp4tProcSpotWeld ArcSpotWeld ClinchWeld Anchor LeftLeaderConnection RightLeaderConnection FilledCircle FilledSquare LargeFilledSquare DatumPoint SnappingDiamond CircleInCircle CircleInSquare SquareInSquare FilledLeftTriangle FilledRightTriangle FilledUpTriangle FilledDownTriangle FilledLeftTriangleInCircle FilledRightTriangleInCircle FilledUpTriangleInCircle FilledDownTriangleInCircle FilledLeftTriangleInSquare FilledRightTriangleInSquare FilledUpTriangleInSquare FilledDownTriangleInSquare RoundedCross FilledDiamond UpDownTriangles LeftRightTriangles SmallWheel LargeWheel HollowCircle PreviewPerpendicular PreviewHorizontal PreviewVertical PreviewTangent PreviewParallel PreviewPointOnCurve PreviewCollinear Ruler Protractor SketchNotebook ArcEndPoint Disp2PtArcMarker BigAsterisk LineInCircle PlusInCircle CenterOfRotation PreviewX PreviewY PreviewZ Disp2tGeneralSpotWeld Disp3tGeneralSpotWeld Disp4tGeneralSpotWeld Disp2tVitalSpotWeld Disp3tVitalSpotWeld Disp4tVitalSpotWeld Disp2tImportantSpotWeld Disp3tImportantSpotWeld Disp4tImportantSpotWeld Disp2tSemipanelSpotWeld Disp3tSemipanelSpotWeld Disp4tSemipanelSpotWeld InvalidMarker -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-