UserDefinedEventReason Enumeration¶
NXOpen.UserDefinedObjects.UserDefinedEvent.Reason is an alias for NXOpen.UserDefinedObjects.UserDefinedEventReason
-
class
NXOpen.UserDefinedObjects.
UserDefinedEventReason
¶ Bases:
object
Available link types for a
UserDefinedObject
.Enum Members
Enum Member Enum Member Description Display Display UDO event Delete An associated object was deleted - UDO cleanup event Update Update UDO event Selection Select UDO event Fit Fit display event AttentionPoint Find Attention Point for the UDO event Info Query UDO Information event Edit Edit UDO event Suppress Suppress/Unsuppress UDO event ScreenSizeFit Fit operation for screen-size geometry -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-