UserDefinedClassSelection Enumeration¶
NXOpen.UserDefinedObjects.UserDefinedClass.Selection is an alias for NXOpen.UserDefinedObjects.UserDefinedClassSelection
-
class
NXOpen.UserDefinedObjects.
UserDefinedClassSelection
¶ Bases:
object
Allow query class from name options for a
NXOpen.UserDefinedObjects.UserDefinedObject
.Enum Members
Enum Member Enum Member Description Off UDO’s of this class will NOT be selectable. On UDO’s of this class will be selectable. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-