UserDefinedClassAllowQueryClass Enumeration¶
NXOpen.UserDefinedObjects.UserDefinedClass.AllowQueryClass is an alias for NXOpen.UserDefinedObjects.UserDefinedClassAllowQueryClass
-
class
NXOpen.UserDefinedObjects.
UserDefinedClassAllowQueryClass
¶ Bases:
object
Allow query class from name options for a
NXOpen.UserDefinedObjects.UserDefinedObject
of this class.Enum Members
Enum Member Enum Member Description Off You do NOT have permission to query the class from it’s name. On You have permission to query the class from it’s name. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-