UpdateFailureOption Enumeration¶
NXOpen.Update.FailureOption is an alias for NXOpen.UpdateFailureOption
-
class
NXOpen.
UpdateFailureOption
¶ Bases:
object
Specifies the action to take when an object fails to update.
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description NoOption No option Undo Perform undo Suppress Suppress failing object SuppressAll Suppress failing objects and subsequent objects Accept Accept failure of failing objects AcceptAll Accept failure of failing objects and subsequent objects Delete Delete failing object DeleteDependents Delete failing object and its dependents Interrupt Interrupt update upon failure -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-