AttachmentAttachType Enumeration¶
NXOpen.UIStyler.Attachment.AttachType is an alias for NXOpen.UIStyler.AttachmentAttachType
-
class
NXOpen.UIStyler.
AttachmentAttachType
¶ Bases:
object
Represents alignment option for Styler Item
Enum Members
Enum Member Enum Member Description Dialog Dialog type Default Default type NotSet None type NoChange No change type Item Item type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-