UIStatus Enumeration¶
NXOpen.UI.Status is an alias for NXOpen.UIStatus
-
class
NXOpen.
UIStatus
¶ Bases:
object
Indicates the Lock, Unlock status of NX functions.
Enum Members
Enum Member Enum Member Description Lock Lock status Unlock Unlock status -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-