NXOpen.UF.View.Lights Structure¶
NXOpen.UF.View.Lights is an alias for NXOpen.UF.ViewLights_Struct
-
class
NXOpen.UF.
ViewLights_Struct
¶ Bases:
object
Refer to UF_VIEW_lights_s for documentation.
Fields
NXOpen.UF.ViewLights_Struct.LightName |
Light name which is limited to 40 characters. |
NXOpen.UF.ViewLights_Struct.LightType |
Lights may be of different types as defined in @@LINK=types.html#UF_VIEW_light_type_e ENDLINK @@ UF_VIEW_light_type_t |
NXOpen.UF.ViewLights_Struct.LightMode |
Specifies whether the light is fixed to the observer or fixed to the part. |
NXOpen.UF.ViewLights_Struct.Location |
Together with ‘to’, determines the direction of the light. |
NXOpen.UF.ViewLights_Struct.To |
Together with ‘location’, determines the direction of the light. |