NXOpen.UF.View.FogOptions Structure¶
NXOpen.UF.View.FogOptions is an alias for NXOpen.UF.ViewFogOptions_Struct
-
class
NXOpen.UF.
ViewFogOptions_Struct
¶ Bases:
object
Refer to UF_VIEW_fog_options_s for documentation.
Fields
NXOpen.UF.ViewFogOptions_Struct.FogMode |
Fog mode in viewThe following constants are valid : UF_VIEW_FOG_OFF, UF_VIEW_FOG_LINEAR, UF_VIEW_FOG_LIGHT and UF_VIEW_FOG_HEAVY |
NXOpen.UF.ViewFogOptions_Struct.FogColor |
Fog color[0] = red, [1] = green, [2] = blue Each color has a range from 0.0 to 1.0. |
NXOpen.UF.ViewFogOptions_Struct.FogFront |
Front fog plane has a range from 0 to 100 and is only valid for fog_mode = UF_VIEW_FOG_LINEAR |
NXOpen.UF.ViewFogOptions_Struct.FogBack |
Back fog plane has a range from 0 to 100 and is only valid for fog_mode = UF_VIEW_FOG_LINEAR. |
NXOpen.UF.ViewFogOptions_Struct.FogRate |
The fog density which has a range from 0 to 100. |