NXOpen.UF.Ugfont.FontHeader Structure¶
NXOpen.UF.Ugfont.FontHeader is an alias for NXOpen.UF.UgfontFontHeader_Struct
-
class
NXOpen.UF.
UgfontFontHeader_Struct
¶ Bases:
object
Refer to UF_UGFONT_font_header_s for documentation.
Fields
NXOpen.UF.UgfontFontHeader_Struct.Version |
This is the internal version number. |
NXOpen.UF.UgfontFontHeader_Struct.Height |
This is the height of the font. |
NXOpen.UF.UgfontFontHeader_Struct.Width |
This is the width of the font. |
NXOpen.UF.UgfontFontHeader_Struct.BaseHeight |
This is the distance to the base line of the characters. |
NXOpen.UF.UgfontFontHeader_Struct.WaistHeight |
This is the distance to the waist line of the characters. |
NXOpen.UF.UgfontFontHeader_Struct.WidthType |
This is the width type of the font: 1 = Fixed width, all characters have the same width. |
NXOpen.UF.UgfontFontHeader_Struct.Overlap1 |
The overlap 1 value |
NXOpen.UF.UgfontFontHeader_Struct.Overlap2 |
The overlap 2 value |
NXOpen.UF.UgfontFontHeader_Struct.Overlap3 |
The overlap 3 value |
NXOpen.UF.UgfontFontHeader_Struct.LineSpacing |
The line spacing of the font. |
NXOpen.UF.UgfontFontHeader_Struct.CharSpacing |
The character spacing of the font. |
NXOpen.UF.UgfontFontHeader_Struct.GridSpacing |
The grid spacing. |
NXOpen.UF.UgfontFontHeader_Struct.NumberOfChars |
This is the total number of characters that are defined in this font. |