NXOpen.UF.Uf.SystemInfo Structure

NXOpen.UF.Uf.SystemInfo is an alias for NXOpen.UF.UfSystemInfo_Struct

class NXOpen.UF.UfSystemInfo_Struct

Bases: object

Refer to UF_system_info_s for documentation.

Fields

NXOpen.UF.UfSystemInfo_Struct.DateBuf Current date and time info
NXOpen.UF.UfSystemInfo_Struct.UserName User, who is running this process
NXOpen.UF.UfSystemInfo_Struct.ProgramName The current program name
NXOpen.UF.UfSystemInfo_Struct.NodeName Machine, on which this process is running
NXOpen.UF.UfSystemInfo_Struct.MachineType Hardware type on which the machine is running
NXOpen.UF.UfSystemInfo_Struct.OsName Operating system, on which this process is running
NXOpen.UF.UfSystemInfo_Struct.OsVersion Version and release level of this Operating System
NXOpen.UF.UfSystemInfo_Struct.PhysicalMemory Returns the number of bytes of physical memory on this machine.
NXOpen.UF.UfSystemInfo_Struct.BundlesUsed Array of the names of the bundles currently in use.
NXOpen.UF.UfSystemInfo_Struct.NumberOfBundles The number of bundles currently in use