NXOpen.UF.Tabnot.SectionPrefs Structure

NXOpen.UF.Tabnot.SectionPrefs is an alias for NXOpen.UF.TabnotSectionPrefs_Struct

class NXOpen.UF.TabnotSectionPrefs_Struct

Bases: object

Refer to UF_TABNOT_section_prefs_s for documentation.

Fields

NXOpen.UF.TabnotSectionPrefs_Struct.HeaderLocation Location to display header
NXOpen.UF.TabnotSectionPrefs_Struct.MaxHeight The maximum height of the section.
NXOpen.UF.TabnotSectionPrefs_Struct.OverflowDirection Direction to overflow sections
NXOpen.UF.TabnotSectionPrefs_Struct.OverflowSpacing Distance to offset continuation sections (only used when table continues on the same sheet)
NXOpen.UF.TabnotSectionPrefs_Struct.AttachPoint Point to which origin is attached
NXOpen.UF.TabnotSectionPrefs_Struct.UseDoubleWidthBorder Should the border be double width?
NXOpen.UF.TabnotSectionPrefs_Struct.BorderWidth Width of border if use_double_width_border is TRUE
NXOpen.UF.TabnotSectionPrefs_Struct.DisplayContinuationNote Display continuation note flag
NXOpen.UF.TabnotSectionPrefs_Struct.ContinuationNote Continuation note string