NXOpen.UF.Studio.StybldShapeTrans Structure¶
NXOpen.UF.Studio.StybldShapeTrans is an alias for NXOpen.UF.StudioStybldShapeTrans_Struct
-
class
NXOpen.UF.
StudioStybldShapeTrans_Struct
¶ Bases:
object
Refer to UF_STUDIO_stybld_shape_trans_s for documentation.
Fields
NXOpen.UF.StudioStybldShapeTrans_Struct.TransType |
Transition type. |
NXOpen.UF.StudioStybldShapeTrans_Struct.Start |
Start value = 0…100. |
NXOpen.UF.StudioStybldShapeTrans_Struct.End |
End value = 0…100. |
NXOpen.UF.StudioStybldShapeTrans_Struct.Peak |
Peak value = 0…100. |
NXOpen.UF.StudioStybldShapeTrans_Struct.Slope |
Slope value = 0…100. |
NXOpen.UF.StudioStybldShapeTrans_Struct.Position |
Position of middle value = 10…90. |