NXOpen.UF.So.OffsetSurfCvtrData Structure

NXOpen.UF.So.OffsetSurfCvtrData is an alias for NXOpen.UF.SoOffsetSurfCvtrData_Struct

class NXOpen.UF.SoOffsetSurfCvtrData_Struct

Bases: object

Refer to UF_SO_offset_surf_cvtr_data_s for documentation.

Fields

NXOpen.UF.SoOffsetSurfCvtrData_Struct.Face object id of the face which contains the evaluation surface
NXOpen.UF.SoOffsetSurfCvtrData_Struct.Uv scalar object ids for the u and v parameters of the surface
NXOpen.UF.SoOffsetSurfCvtrData_Struct.Option flag for evaluation option: 0 = u isoparametric 1 = v isoparametric 2 = section
NXOpen.UF.SoOffsetSurfCvtrData_Struct.Secdir object id of the section direction