NXOpen.UF.So.DirrOnSurfData Structure¶
NXOpen.UF.So.DirrOnSurfData is an alias for NXOpen.UF.SoDirrOnSurfData_Struct
-
class
NXOpen.UF.
SoDirrOnSurfData_Struct
¶ Bases:
object
Refer to UF_SO_dirr_on_surf_data_s for documentation.
Fields
NXOpen.UF.SoDirrOnSurfData_Struct.Face |
object id of the face which contains the evaluation surface |
NXOpen.UF.SoDirrOnSurfData_Struct.Uv |
scalar object ids for the u and v parameters of the surface |
NXOpen.UF.SoDirrOnSurfData_Struct.Option |
flag for evaluation option: 0 = u isoparametric 1 = v isoparametric 2 = surface normal 3 = section |
NXOpen.UF.SoDirrOnSurfData_Struct.Secdir |
object id of the section direction |
NXOpen.UF.SoDirrOnSurfData_Struct.Flip |
flag for direction reversal 0 = no 1 = yes |