NXOpen.UF.Smd.SeqOutput Structure¶
NXOpen.UF.Smd.SeqOutput is an alias for NXOpen.UF.SmdSeqOutput_Struct
-
class
NXOpen.UF.
SmdSeqOutput_Struct
¶ Bases:
object
Refer to UF_SMD_seq_output_s for documentation.
Fields
NXOpen.UF.SmdSeqOutput_Struct.DesignAngle |
Design angle of the feature. |
NXOpen.UF.SmdSeqOutput_Struct.ProcessAngle |
Process angle of the feature. |
NXOpen.UF.SmdSeqOutput_Struct.InsideRadius |
Inside radius of the feature. |
NXOpen.UF.SmdSeqOutput_Struct.BendAllowance |
Dimensional amount added to feature during the elongation process. |
NXOpen.UF.SmdSeqOutput_Struct.Feature |
Feature on which the process is performed. |
NXOpen.UF.SmdSeqOutput_Struct.FeatureName |
Unigraphics proper name of the feature. |
NXOpen.UF.SmdSeqOutput_Struct.ProcessName |
Name of the process in the forming table. |
NXOpen.UF.SmdSeqOutput_Struct.BendDirection |
The direction(up/down) of the bend. |
NXOpen.UF.SmdSeqOutput_Struct.Description |
Description of process in the forming table. |
NXOpen.UF.SmdSeqOutput_Struct.Baf |
Bend Allowance Formula. |