NXOpen.UF.Smd.SeqInput Structure

NXOpen.UF.Smd.SeqInput is an alias for NXOpen.UF.SmdSeqInput_Struct

class NXOpen.UF.SmdSeqInput_Struct

Bases: object

Refer to UF_SMD_seq_input_s for documentation.

Fields

NXOpen.UF.SmdSeqInput_Struct.ProcessAngle Process angle of the feature.
NXOpen.UF.SmdSeqInput_Struct.Feature Feature on which the process is performed.
NXOpen.UF.SmdSeqInput_Struct.ProcessName Name of the process in the forming table.
NXOpen.UF.SmdSeqInput_Struct.ProcessType Type of the process in the forming table.
NXOpen.UF.SmdSeqInput_Struct.Description Description of process in the forming table.