NXOpen.UF.Smd.GenPrefs Structure¶
NXOpen.UF.Smd.GenPrefs is an alias for NXOpen.UF.SmdGenPrefs_Struct
-
class
NXOpen.UF.
SmdGenPrefs_Struct
¶ Bases:
object
Refer to UF_SMD_gen_prefs_s for documentation.
Fields
NXOpen.UF.SmdGenPrefs_Struct.SeqLabels |
Display sequence labels on body 0 = Do not display the labels. |
NXOpen.UF.SmdGenPrefs_Struct.UseFeatStds |
Use feature standards on dialogs (1/0) |
NXOpen.UF.SmdGenPrefs_Struct.ChkStds |
Check standards on create (1/0) |
NXOpen.UF.SmdGenPrefs_Struct.DefaultBaf |
Bend Allowance formula for the creation of flat patterns & unformed bodies. |
NXOpen.UF.SmdGenPrefs_Struct.Material |
Material type of the body. |
NXOpen.UF.SmdGenPrefs_Struct.Thickness |
Material thickness of the body |
NXOpen.UF.SmdGenPrefs_Struct.LineColor |
Reference line color |
NXOpen.UF.SmdGenPrefs_Struct.EnforceCreState |
Enforce Creation State Editing |
NXOpen.UF.SmdGenPrefs_Struct.MatMargin |
Percentage by which bracket is made larger |
NXOpen.UF.SmdGenPrefs_Struct.UseBat |
OBSOLETE. |
NXOpen.UF.SmdGenPrefs_Struct.UseGlobalThickness |
Use Global thickness for feature creation (True/ False) |
NXOpen.UF.SmdGenPrefs_Struct.ThicknessType |
Thickness type 0 - Infer the thickness 1 - Use Expression |
NXOpen.UF.SmdGenPrefs_Struct.UseGlobalRadius |
Use global radius for feature creation (True / False ) |
NXOpen.UF.SmdGenPrefs_Struct.GlobalRadius |
Global radius |
NXOpen.UF.SmdGenPrefs_Struct.RadiusType |
Radius typeUF_SMD_RADIUS_INSIDE UF_SMD_RADIUS_OUTSIDE |
NXOpen.UF.SmdGenPrefs_Struct.UseGlobalAngle |
Use global angle value for feature creation (True / False) |
NXOpen.UF.SmdGenPrefs_Struct.GlobalAngle |
Global angle value |
NXOpen.UF.SmdGenPrefs_Struct.AngleType |
Angle typeUF_SMD_ANGLE_INCLUDED UF_SMD_ANGLE_BEND |
NXOpen.UF.SmdGenPrefs_Struct.BafOption |
Options for BAFUF_SMD_BAF_USE_EXPRESSION UF_SMD_BAF_USE_TCL UF_SMD_BAF_USE_SPRDSHEET |
NXOpen.UF.SmdGenPrefs_Struct.UseGlobalBaf |
Use global BAF for feature creation (True / False ) |
NXOpen.UF.SmdGenPrefs_Struct.FormingMethod |
Forming methodUF_SMD_USE_SELF_FORMING_FEATURES, UF_SMD_USE_FORMING_OPERATIONS |
NXOpen.UF.SmdGenPrefs_Struct.BatRadiusType |
Radius typeUF_SMD_BAT_RADIUS_INSIDE UF_SMD_BAT_RADIUS_OUTSIDE |
NXOpen.UF.SmdGenPrefs_Struct.BatAngleType |
Angle typeUF_SMD_BAT_ANGLE_INCLUDED UF_SMD_BAT_ANGLE_BEND |
NXOpen.UF.SmdGenPrefs_Struct.PipSequential |
PIP sequential Processing UF_SMD_NON_SEQUENTIAL_PROCESS, UF_SMD_SEQUENTIAL_PROCESS |