NXOpen.UF.Smd.FpPrefs Structure¶
NXOpen.UF.Smd.FpPrefs is an alias for NXOpen.UF.SmdFpPrefs_Struct
-
class
NXOpen.UF.
SmdFpPrefs_Struct
¶ Bases:
object
Refer to UF_SMD_fp_prefs_s for documentation.
Fields
NXOpen.UF.SmdFpPrefs_Struct.AngleTol |
The angle tolerance to use in laying out the surfaces |
NXOpen.UF.SmdFpPrefs_Struct.ChordTol |
The chordal tolerance to use in mapping curves to the flat pattern |
NXOpen.UF.SmdFpPrefs_Struct.GridSize |
Grid size |
NXOpen.UF.SmdFpPrefs_Struct.Layer |
Layer to place flat pattern on |
NXOpen.UF.SmdFpPrefs_Struct.DistortionConstraint |
Controls distortion face mapping (Longest edge / Shortest edge) |
NXOpen.UF.SmdFpPrefs_Struct.FpOrientation |
Enumerated type defining where to create the flat pattern |
NXOpen.UF.SmdFpPrefs_Struct.CurveSet |
Enumerated type defining which curves are used to generate a Flat Pattern. |
NXOpen.UF.SmdFpPrefs_Struct.TangentLines |
Bend Tangent lines created on theFlat Pattern (TRUE/FALSE). |
NXOpen.UF.SmdFpPrefs_Struct.CenterLines |
Bend Center lines created on the Flat Pattern (TRUE/FALSE). |
NXOpen.UF.SmdFpPrefs_Struct.FormBlockCurves |
Form Block curves created on the Flat Pattern (TRUE/FALSE). |
NXOpen.UF.SmdFpPrefs_Struct.ContourCurves |
Contour curves created on the Flat Pattern (TRUE/FALSE). |
NXOpen.UF.SmdFpPrefs_Struct.MultipleFp |
Allow multiple flat patterns (TRUE/FALSE). |
NXOpen.UF.SmdFpPrefs_Struct.AutoUpdate |
Enable auto flat pattern update |
NXOpen.UF.SmdFpPrefs_Struct.UseBaf |
Use BAF when creating flat pattern |
NXOpen.UF.SmdFpPrefs_Struct.Name |
Default flat pattern name |
NXOpen.UF.SmdFpPrefs_Struct.FpAlgorithm |
Flat Pattern Creation algorithm |