NXOpen.UF.Sket.ConGeom Structure

NXOpen.UF.Sket.ConGeom is an alias for NXOpen.UF.SketConGeom_Struct

class NXOpen.UF.SketConGeom_Struct

Bases: object

Refer to UF_SKET_con_geom_s for documentation.

Fields

NXOpen.UF.SketConGeom_Struct.GeomTag The geomtry’s tag
NXOpen.UF.SketConGeom_Struct.VertexType Vertex type if it is the vertex of the geometry that will be constrained.
NXOpen.UF.SketConGeom_Struct.VertexIndex Starting from 1.
NXOpen.UF.SketConGeom_Struct.UseHelp Whether to use help data (either help points or help parameter.) Valid types as specified in UF_SKET_help_type_t.
NXOpen.UF.SketConGeom_Struct.HelpPoint Help point
NXOpen.UF.SketConGeom_Struct.HelpParameter Help parameter